This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

为什么我的uart发送和收到的数据不一致??请教



#include <stdint.h>

#include <stdbool.h>

#include "inc/hw_ints.h"

#include "inc/hw_memmap.h"

#include "inc/hw_types.h"

#include "driverlib/debug.h"

#include "driverlib/fpu.h"

#include "driverlib/gpio.h"

#include "driverlib/interrupt.h"

#include "driverlib/sysctl.h"

#include "driverlib/uart.h"

#include "driverlib/rom.h"

#include "driverlib/pin_map.h"

 

//串口接收中断服务程序

void UARTIntHandler(void)

{

  ui32 ulStatus;

  //获取中断状态

  ulStatus = ROM_UARTIntStatus(UART0_BASE, true);

  //清除中断标志

  ROM_UARTIntClear(UART0_BASE, ulStatus);

  //直到串口FIFO中没有数据时才退出循环

  while(ROM_UARTCharsAvail(UART0_BASE))

  {

      //读串口接收的字符并回发

      ROM_UARTCharPutNonBlocking(UART0_BASE,

             ROM_UARTCharGetNonBlocking(UART0_BASE));

  }

 }

 

//串口发送函数

void  UARTSend(const ui8 *pucBuffer, ui32 ulCount)

{

  while(ulCount--)

  {

      //将要发送的字符写进UART

      ROM_UARTCharPutNonBlocking(UART0_BASE, *pucBuffer++);

  }

}

 

int main(void)

{

  //使能FPU

  FPUEnable();

  FPULazyStackingEnable();

 

  //设置时钟直接使用外部晶振

  ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC |

                SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

 

  //使能用到的外设

  ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

  ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

  //配置PA0和PA1为串口0引脚

  ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 |

                         GPIO_PIN_1);

 

  //使能中断

  ROM_IntMasterEnable();

 

  //配置UART0为115200,8-N-1

  ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(),

                            115200, (UART_CONFIG_WLEN_8 |

          UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

  //使能串口中断

  ROM_IntEnable(INT_UART0);

  ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);

  //发送提示信息

  UARTSend((ui8 *)"Enter text: \r", 13);

 

  while(1)

  {

   }

  }

 

 

 

 

这个是我得程序,为什么会这样,我用的串口调试助手,电脑给板子发,让他受到什么回发什么,而且我也让板子发出一条消息,可那条消息电脑跟本收不到,

 例如:发送22受到33 ,发11受到00,发55受到 44,发aa受到bb,发00还收到00,发33受到33 ,发44受到44,波特率电脑和板一样,没有采用校验,用的usb转232(转换芯片pl2302),芯片没问题 我在另一种板子上试了,串口调试助手我也换了好几个了结果一样