This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我们在使用MSP432E401Y LaunchPad开发套件结合Scalable PMICs GUI对TSP6593Q1进行测试验证时,首先将USB线缆连接至XDS110端后下载XDS110驱动安装,电脑设备管理器可以正确识别到XDS110端的串口,如下图所示:
随后在英文论坛与其他帖子中了解到,需要通过XDS110端口给MSP432E401Y芯片烧写固件,于是通过UNIFlash给MSP432E401Y烧写了版本为1.0.3.6的固件,并且可以正常通过UNIFlash软件访问其内存,如下图所示:
在下载完固件以后需要将USB线缆插入U7,即靠近MSP432E401Y芯片侧的USB端口,并将JP1切换至中间导通与外部供电3.3V,如下图所示:
理论上在电脑的设备管理器其他设备处会出现一个Virtual com port,此后Scalable PMICs GUI软件就会读取到硬件平台,但是电脑设备管理器却没有任何反应,上位机也无法正常读取到硬件平台,如下所示:
目前经过测量,硬件供电电压正常,芯片可正常发热,晶振正常起振,并可利用XDS110访问芯片内存与Flash,硬件上暂未发现问题。
目前已尝试过的解决方法有:
1.两端同时连接USB线缆
2.在MSP432E401Y供电时断开XDS110部分的供电
3.采用外置5V稳压源供电
4.换更换电脑进行尝试
5.更换安装版Scalable PMICs GUI软件至网页版
6. 重新烧写1.0.3.6固件
7.采用网线进行连接
8.更换USB数据线缆
均无法解决此问题,实际上在第一次烧写固件并更换USB线缆连接后,在电脑设备管理器栏的其他设备里短暂出现过一次Virtual com port,但是似乎并不稳定,在约几分钟后消失,此后并再没成功出现过吗,请问有无方法解决此问题?谢谢。
现在我下载了一个CCS软件,并尝试将其中的实例工程中的代码下载进入MSP432E401Y LaunchPad中,所有的程序下载都没有问题显示成功,我一共尝试了两种类型的代码,其中在TI Driver目录下的gpiointerrupt工程在下载完成后可以通过控制按钮来控制板载LED灯的亮灭,但是所有与USB有关的工程在下载后连接电脑都没有反应,包括模拟虚拟端口、键盘模拟和鼠标模拟的工程,于是我猜测可能是硬件上连接不稳定导致的,在使用万用表确认USB端口连接没问题后,并补充了PL6和PL7引脚的锡,重新上电依然没有反应。
你好,参考下工程师的回复:
目前的问题并不完全是 PMIC 本身,而是MSP432E401Y LaunchPad 开发套件,对吗?
最终目标是能够在客户主板上验证 TPS6593Q1,对吗?
您能否链接引导您找到固件的论坛帖子以及显示可扩展 PMIC GUI 软件可以交互的说明?
是的,目前的问题就是MSP432E401Y LaunchPad 开发套件无法连接至电脑的问题,最终是想通过launchpad烧写程序至PMIC里进行电源验证后在项目中使用(如果有其他办法的话可以帮忙推荐下,谢谢),帖子的链接如下:MSP432E401Y: MSP432E401Y: How can I get firmware version 1.0.3.6 for msp-exp432e401y - Power management forum - Power management - TI E2E support forums
现在烧写LED灯闪烁例程和GPIO中断例程后无反应,重新烧写1.0.3.6的固件后插入USB线缆,在电脑上的设备管理器部分则会一直显示stellaris device firmware upgrade,更换电脑后则显示Tiva device firmware update,在恢复出厂设置操作(链接:Using SimpleLink MSP432E4 microcontrollers over the JTAG interface (Rev. A) (ti.com))后重新烧写依然不变。
你好,参考下工程师的回复:
please allow for some time to look this all over.
As of right now we no longer offer the MSP432E401Y LaunchPad development kit method in order to connect to the GUI, but no instead is an integrated MSP432 on the evaluation modules, we do have methods that show how to use these EVMs to communicate to PMICs already on development boards.
You asked for another method, and there's one alternative above.
Still we'll try to get launchpad up and running.