Part Number: MSPM0L1306
我在基于MSPM0L1306芯片上开发UART代码,想使用重载fputc来最终支持将printf函数重定向到UART输出。目前做了如下尝试:
1、如附件所示,编辑了C代码,在基于Keil构建的MSPM0L1306工程,目前测试是可以实现将printf函数重定向到UART输出的。
2、但在用CCS12.5下,使用同样的C代码,编译下载运行,所有的printf是不起作用的。
想咨询如何修改CCS工程配置或者修改C代码,达到支持printf函数重定向到UART上?
/*
* Copyright (c) 2023, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
// To Using Chinese correctly on UART, please use GBK encoding.
#include "ti_msp_dl_config.h"
#include "string.h"
#include "stdio.h"
#define LineLength 64
/* This results in approximately 10ms of delay assuming 32MHz CPU_CLK */
#define DELAY (320000)
#if 1
//#pragma import(__use_no_semihosting)
//������Ҫ��֧�ֺ���
//struct __FILE
//{
// int handle;
//};
FILE __stdout;
//����_sys_exit()�Ա���ʹ�ð�����ģʽ
void _sys_exit(int x)
{
x = x;
}
//�ض���fputc����
int fputc(int ch, FILE *f)
{
DL_UART_Main_transmitDataBlocking(UART_0_INST, ch);
return ch;
}
#endif
// UART Received Buffer, Max Length = LineLength
volatile uint8_t LineBuffer[LineLength];
// Flag for the UART Received Status
// Bit15 - Finished for Received One Line
// Bit14 - Got '\r' Flag
// Bit13 ~ Bit0 - The Length of the Received Char
volatile uint16_t UART_RX_STA = 0;
int main(void)
{
unsigned short times = 0;
unsigned short len;
unsigned short n;
/* Power on GPIO, initialize pins as digital outputs */
SYSCFG_DL_init();
/* Default: LED1 OFF */
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN );
NVIC_ClearPendingIRQ(UART_0_INST_INT_IRQN); //Clear the IRQ Flag
NVIC_EnableIRQ(UART_0_INST_INT_IRQN); //Enable the Received Interrupt
while (1) {
if(UART_RX_STA & 0x8000) //check the received finish flag
{
len = UART_RX_STA & 0x3FFF; //Got the Length of the received
printf("\r\n�����͵���ϢΪ:\r\n");
//Send the received Line
for(n=0; n<len; n++)
DL_UART_Main_transmitDataBlocking(UART_0_INST, LineBuffer[n]);
printf("\r\n\r\n");
UART_RX_STA = 0; //Clear the Flag of the Received
}
else {
times ++;
if(times % 5000 == 0) //Per 50S
{
printf("\r\nMSPM0+ UART����ʵ��\r\n");
printf("HardwareLab@���пƴ�\r\n");
}
if(times %200 == 0) printf("���������ݣ��Իس�����: \r\n"); //Per 2S
if(times % 30 == 0) DL_GPIO_togglePins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN ); //Per 300ms
delay_cycles(DELAY);
}
}
}
volatile uint8_t gRxData = 0;
void UART_0_INST_IRQHandler(void)
{
switch (DL_UART_Main_getPendingInterrupt(UART_0_INST)) {
case DL_UART_MAIN_IIDX_RX:
gRxData = DL_UART_Main_receiveData(UART_0_INST);
if((UART_RX_STA & 0x8000)==0) //Receive Not Finished
{
if(UART_RX_STA&0x4000) //Received 0x0D('\r')
{
if(gRxData!=0x0a)UART_RX_STA=0; //Received Error
else UART_RX_STA|=0x8000; //Received Finished
}
else //Not Got 0x0D('\r')
{
if(gRxData==0x0d)UART_RX_STA|=0x4000;
else
{
LineBuffer[UART_RX_STA&0X3FFF]=gRxData ; // Got One Valid Char
UART_RX_STA++;
if(UART_RX_STA>(LineLength-1))UART_RX_STA=0; //Received Error, Restart Again
}
}
}
break;
default:
break;
}
}