我在基于MSPM0L1306芯片上开发UART代码,想使用重载fputc来最终支持将printf函数重定向到UART输出。目前做了如下尝试:
1、如附件所示,编辑了C代码,在基于Keil构建的MSPM0L1306工程,目前测试是可以实现将printf函数重定向到UART输出的。
2、但在用CCS12.5下,使用同样的C代码,编译下载运行,所有的printf是不起作用的。
想咨询如何修改CCS工程配置或者修改C代码,达到支持printf函数重定向到UART上?
/*
 * Copyright (c) 2023, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */
// To Using Chinese correctly on UART, please use GBK encoding.
#include "ti_msp_dl_config.h"
#include "string.h"
#include "stdio.h"
#define LineLength  64
/* This results in approximately 10ms of delay assuming 32MHz CPU_CLK */
#define DELAY (320000)
#if 1
//#pragma import(__use_no_semihosting)             
//������Ҫ��֧�ֺ���                 
//struct __FILE 
//{ 
//	int handle; 
//}; 
FILE __stdout;       
//����_sys_exit()�Ա���ʹ�ð�����ģʽ    
void _sys_exit(int x) 
{ 
	x = x; 
} 
//�ض���fputc���� 
int fputc(int ch, FILE *f)
{ 	
	DL_UART_Main_transmitDataBlocking(UART_0_INST, ch);
	return ch;
}
#endif 
// UART Received Buffer, Max Length = LineLength
volatile uint8_t LineBuffer[LineLength];
// Flag for the UART Received Status
// Bit15 - Finished for Received One Line
// Bit14 - Got '\r' Flag
// Bit13 ~ Bit0 - The Length of the Received Char
volatile uint16_t UART_RX_STA = 0;
int main(void)
{
    unsigned short times = 0;
    unsigned short len;
    unsigned short n;
    /* Power on GPIO, initialize pins as digital outputs */
    SYSCFG_DL_init();
    /* Default: LED1 OFF */
    DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN );
    NVIC_ClearPendingIRQ(UART_0_INST_INT_IRQN);     //Clear the IRQ Flag
    NVIC_EnableIRQ(UART_0_INST_INT_IRQN);           //Enable the Received Interrupt
    while (1) {
        if(UART_RX_STA & 0x8000)    //check the received finish flag
        {
            len = UART_RX_STA & 0x3FFF; //Got the Length of the received
            printf("\r\n�����͵���ϢΪ:\r\n");
            //Send the received Line
            for(n=0; n<len; n++)
                DL_UART_Main_transmitDataBlocking(UART_0_INST, LineBuffer[n]);
            printf("\r\n\r\n");
            UART_RX_STA = 0;    //Clear the Flag of the Received
        }
        else {
            times ++;
            if(times % 5000 == 0)   //Per 50S
            {
                printf("\r\nMSPM0+ UART����ʵ��\r\n");
                printf("HardwareLab@���пƴ�\r\n");
            }
            if(times %200 == 0) printf("���������ݣ��Իس�����: \r\n");  //Per 2S
            if(times % 30 == 0) DL_GPIO_togglePins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN );  //Per 300ms
            delay_cycles(DELAY);
        }
    }
}
volatile uint8_t gRxData = 0;
void UART_0_INST_IRQHandler(void)
{
    switch (DL_UART_Main_getPendingInterrupt(UART_0_INST)) {
        case DL_UART_MAIN_IIDX_RX:
            gRxData = DL_UART_Main_receiveData(UART_0_INST);
            if((UART_RX_STA & 0x8000)==0)  //Receive Not Finished
            {
                if(UART_RX_STA&0x4000) //Received 0x0D('\r')
                {
                    if(gRxData!=0x0a)UART_RX_STA=0;   //Received Error
                    else UART_RX_STA|=0x8000;  //Received Finished
                }
                else //Not Got 0x0D('\r')
                {
                    if(gRxData==0x0d)UART_RX_STA|=0x4000;
                    else
                    {
                        LineBuffer[UART_RX_STA&0X3FFF]=gRxData ;    // Got One Valid Char
                        UART_RX_STA++;
                        if(UART_RX_STA>(LineLength-1))UART_RX_STA=0;   //Received Error, Restart Again
                    }
                }
            }
            break;
        default:
            break;
    }
}