This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: 两个外部晶振是否可以去掉其中一个,另外一个时钟是否可以校准内部的两个时钟

Part Number: MSPM0G3507

MCU原理图设计给出两个外部晶振作为时钟源输入,考虑只加一个外部时钟即32MHz的晶振作为单一时钟源的输入是否可以校准内部低速时钟电路,或者会对MCU在使用时尤其是定时器和RTC时钟会产生哪些影响,对好的建议是什么

  • 您好

    在MSPM0G3507 MCU的设计中,如果原理图原本设计有两个外部晶振作为时钟源输入,一个可能是32MHz的晶振用于高速时钟(如系统时钟、CPU时钟等),而另一个32.768kHz的晶振通常用于实时时钟(RTC)或低功耗模式时的时钟源。

    如果只使用一个32MHz的外部晶振作为单一时钟源输入,那么会面临以下几个问题和影响:

    1. RTC功能受限:RTC通常需要一个非常稳定和精确的时钟源,通常使用32.768kHz晶振。如果去掉这个晶振,RTC的精度和稳定性将无法得到保证,可能导致时间偏差较大,这对于需要精确时间的应用(如数据记录、时间戳等)来说是不可接受的。

    2. 定时器精度:虽然32MHz晶振可以用于MCU内部的高速定时器,但低速定时器(如用于睡眠唤醒或周期性任务的定时器)的精度可能会受到影响,因为它们可能依赖于内部低速时钟电路。这些内部低速时钟电路可能无法通过32MHz晶振进行精确校准。

    3. 低功耗模式受限:在低功耗模式下,MCU通常会切换到使用低速时钟源来降低功耗。如果只有32MHz晶振,MCU可能无法进入某些低功耗模式,或者即使进入也无法保持预期的功耗水平。

    4. 软件兼容性和复杂性:如果只使用一个32MHz晶振,可能需要在软件中进行额外的处理来模拟或补偿RTC和低速定时器的功能。这可能会增加软件的复杂性和出错的可能性。

    建议:

    • 如果应用对RTC和低速定时器的精度要求不高,或者可以通过软件校准和补偿来接受一定的误差,那么可以考虑只使用一个32MHz晶振。但请确保在设计和测试阶段充分评估这些影响。

    • 如果应用对RTC和低速定时器的精度有严格要求,那么建议保留32.768kHz晶振。这可以确保RTC和低速定时器的稳定性和精度,同时减少软件复杂性和出错的可能性。

    • 如果可能的话,考虑使用MCU内部的PLL(相位锁定环)或其他时钟生成器来从32MHz晶振生成所需的低速时钟信号。但请注意,这可能需要额外的硬件和软件支持,并且可能无法完全替代外部低速晶振的精度和稳定性。

    综上官方不建议您去掉其中一个外部时钟。当然如果您如建议中的相关情况,请您根据建议根据您实际情况进行调整,官方不推荐去掉外部时钟。