Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

以上是左边是boot跳转app的代码截图,右边是app的代码
代码运行跳转到app后,运行app初始化后打印出一段“main sta”log后(没有打印完全),就自动复位重启了
这个是不是哪里还需要设置,能否提供一下boot跳转到app的参考说明以及注意点
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

以上是左边是boot跳转app的代码截图,右边是app的代码
代码运行跳转到app后,运行app初始化后打印出一段“main sta”log后(没有打印完全),就自动复位重启了
这个是不是哪里还需要设置,能否提供一下boot跳转到app的参考说明以及注意点

这个bsl_software_invoke_app_demo_uart示例只是跳转到rom的bsl的把?现在secondary bsl的例程是从0x1000开始的,我是否需要修改这段代码,怎么修改?
e2e.ti.com/.../4994050这上面只是提示了app与bootloader的具体地址分配
您好
给您发的E2E帖子里面有告诉您secondary bsl的流程,secondary BSL is placed from 0x1000 to 0x3000. In the sysconfig of the demo code, you can find that the 0x1000 ~0x3000 is statically write protected. And the application code is placed from 0x3000 ~.
说的就是这个图片中的结构

secondary BSL的流程是这样的

Secondary Bootloader Example也有描述This example takes care of secondary bootloader implementation as well as the registration of it. Hence once this image is loaded to the device, the primary bootloader in the device can't be used. Only the secondary Bootloader will be active.
您好
为更加有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上(TI E2E support forums),将由资深的英文论坛工程师为您提供帮助