This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316A: Speed Input Mode Select

Part Number: MCT8316A

当Speed Input Mode Selec t选择 pwm speed input mode 时,选择用20Khz频率的PWM作为输入,运行时,电机会有时不时的卡顿一下,然后有正常运行,当将PWM的频率降低至10Khz时,此现象消失,请问这是什么原因?

看datasheet上面的PWM输入最高可以到95Khz。请问:如果还是用20Khz的PWM作为输入,如何消除卡顿现象?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • PWM频率会影响电机的电流纹波和扭矩输出,电流调节不稳定,从而引起转矩波动和卡顿。

    也可以用示波器​​检查一下输入到MCT8316A的PWM信号质量,信号质量不好可能导致信号​​上升/下降沿不够陡峭,当频率升高时这种畸变可能更严重。

    有条件可以买个开发板对比测试一下,有助于更快找到问题原因

    MCT8316AEVM