Part Number: DRV8163S-Q1EVM
Other Parts Discussed in Thread: DRV8163-Q1
Hi,
I need to use 2x DRV8163S for BDC motor driving. The SPI version offers rich fault diagnosis functions. My questions are:
What is the functional safety level of the DRV8163S? Does it meet ASIL-B?
I am implementing a full-bridge DRV8163S using 2x half-bridge DRV8163S. My functional safety goal is to achieve ASIL-B level for fault/unintended motor drive. Can I meet my ASIL-B level requirement using SPI (internal fault diagnosis mechanism)? This means without adding an additional FET short-circuit fault diagnosis mechanism, only implementing FET fault diagnosis through the chip's internal FET short-circuit fault diagnosis mechanism and reading the data via SPI.
Best regards,
Xiaoshan Lu