This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti工程师,
DRV8824驱动步进电机,当步进电机到转动到外部增加的结构限制点位的时候,因为堵转,8824是否会停止驱动步进电机,或者是是否有反馈信号给出,以方便主控MCU控制步进电机停下。
引脚6、9接的电阻是否是限制DRV8824最大驱动电流的,电阻的选择对功耗是否有要求需要大封装的。
引脚18脚nFault 这个过流返回一个低电平,这个过流是指最大1.6A的电流还是我通过6.9脚设置的驱动电流?
DRV8824没有堵转检测功能,请换DRV8889或DRV8434A/S。
电流检测电阻采样电流,用来做定电流驱动,需要使用大功率封装。
指内置的OCP保护电流,不是你设定的定电流。