This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用DRV8846制作了一批电机驱动;
硬件电路是严格按照手册给出的典型电路搭建的;
机器有开机过程和命令电机旋转过程;
软件配置为32细分,75%电流,衰减模式为手动,Toff为高阻。反复开关机,并命令电机旋转,电机表现为可能声音很轻,也可能噪音很重,并且电机抖动,出现噪音概率很大,;如果开机后声音很轻,只要不关机,声音一直很轻;如果开机后电机噪音大,只要不关机,噪音一直很大;
电机的噪音文件:
电机异响时AOUT1处的波形为:
软件做修改:机器开机后衰减模式自动,Toff高阻;命令电机运行前,把衰减模式改为手动,短时间反复测试,声音很轻,没有噪音。
如果不做软件修改,使用热风枪重新焊接DRV8846,短时间反复测试也没有出现电机噪音很大的情形。
请问此现象是与软件的配置有关还是与芯片的焊接有关。
郑工,手上没有直接测试电流的工具,不知道测试AISEN和BISEN对地电阻两端的电压是不是可以分析,对地电阻值为0.4欧姆。这是电机异响时的波形
这是电机没有异响时的波形
从波形上看,异响确实源于波形失真。电流下降时出现的失真一般可以通过强制快衰减模式或者提高Toff时间来改善。DRV8846本身也是有auto-tune模式可以试一下。