This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8821: 输出电流无变化

Part Number: DRV8821


我们用了DRV8821的步进电机驱动芯片,现在调试时发现了这个问题:

调整Vref的电压,从1.0V到3.5V,电机的输出电流都没有变化(从输入电源的功率来比较)。

我们的要达到的目的是,Vref设为2.4至3V间,在电机转动时输出电流在1.2到1.5A之间,电机不转动时,Vref 降为1V,输出电流在0.5A左右,以降低能耗。

下面是我们的电路原理图:

如果我们设计中有哪些不对的地方,请指正