1、电机转动中,IN1和IN2同时输入高,使电机刹车,但电机并不会按照期望的进行刹车,此时FAULTn脚能检测到被拉低。
2、当芯片处于IN1和IN2同时输入高的初始状态时,拉低其中一个引脚,电机并不能启动。只有初始状态为IN1、IN2同时输入低时,拉高其中一个引脚,才能使电机转动。
3、如果将ISENSE引脚直接接地,此时尝试启动电机,电机无法启动,并且FAULTn脚能检测到被拉低。
4、当IN1、IN2输入为一高一低正常控制电机转动过程中,有一定概率电机异常停止,用示波器测试IN1、IN2的输入没有变化 但OUT1、OUT2不再输出电压。且此现象只会出现在电机某一个转动方向上,而不是两个方向的转动都可能会出现电机异常停止。当电机异常停止时,FAULTn脚可能输出低,也可能仍旧是高阻态。