This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We've got the issue and escalated to E2E for more help, please expect the response.
Thanks.
Hi,
Ae you using Hall ICs in your motor? We see these type of issues when the HALL IC configurations are incorrect. Can you refer to section 9.1.1 in the datasheet?
FR is direction control. When low, phase driving sequence is U → V → W. When high, the phase driving sequence is U → W → V.
CMTMOD configuration depends on Hall placement and commutation type. Pull low for sinusoidal operation mode with 0° Hall placement, High for sinusoidal mode with 30° Hall placement and floating for Trapezoidal operation mode with 30° Hall placement
Make sure BRKMOD is pulled low for normal operation.
Is RD pin indicating a fault? Make sure CS resistor (as mentioned in section 8.3.1) is configured to set the right current limit. Setting Rcs to lower current limit can trigger a current limit fault.
Thanks.
hello,thanks for your help,but I want ask a question, for example How to judge whether the chip is burnt out? When VM supplies 12V voltage, VINT should output 5V voltage, right? If VINT does not input 5V voltage, can it be considered that the chip is broken
Hi,
Yes, if the device fails to output 5V at VINT, then the device is damaged.
Thanks.
Hi,
I have successfully used the drv10970 drive motor, but I encountered a new problem. When using the drv10970 drive motor to realize closed-loop PID control, the motor rotates too laggy, that is, the motor rotates very incoherently,PWM is set to 20KHz。
Thanks.
Hi,
There is no closed loop PI controller in the device. is this closed loop implemented externally?
Hi,
Yes,sir,An encoder is installed to feed back data to STM32 to realize closed-loop control,and The frequency of PMW is 20kHz. When the duty cycle of PWM is lower than about 20%, the motor will jitter. When the duty cycle of PWM is higher than about 20%, the motor operates normally
Hi,
Since speed loop is not part of this device, we can't really tell why there is speed jitter. Can you try adjusting the speed PI controller gains?
Thanks.