This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在正常测试条件下,采用外接控制板来控制,多次测量都没有问题,偶然一次出现断电前工作正常,断电后过了几分钟再次使用就出现问题了,测量C7、C8电容短路,C2、C3电容的容值变成100uf左右,且芯片的第10脚STEP_AIN1对GND短路(开始没测过,不知道是不是正常的)。
您好,
要想使外部信号连接到 EVM,需要移除驱动器和 MCU 之间的连接。 如果 STEP_AIN1来自外部信号,那么应移除 J6上的分流器,以免其与 MCU 发生碰撞。
好的,现在的情况是将芯片从电路板上取下后C7、C8不短路了,基本可以肯定的是芯片的两个引脚对地短路了,现在我买了一片新的芯片换上后短路的地方已经恢复了,但是C2、C3电容在电路板上的测量值是100uf多,是因为几个电容并联导致的吗?,0x04寄存器的DECMOD我这设置成Force fast decay at all times或Use mixed decay at all times这两种,会对设备造成影响吗
我们一起问下,我把英文论坛的链接也给您放上来,您可以看下,因为我个人原因,这周内可能没办法及时转达给您工程师的答复:
e2e.ti.com/.../drv8711evm-abnormal-behavior-after-power-down