DRV8870 外部条件:原理图设计和手册要求一致,电流限制为1.3A,使用8KHz PWM 85%~100%占空比驱动IN1,IN2低电平。 驱动一个直流有刷电机,如果驱动线比较短(15cm),运行比较正常(速度30RPM),稍微加长几个cm,电机速度就变为几乎不动了,测量OUT1波形,发现只有大约20us为高电平,正常应该有100us高电平,不知道为啥会这样。




This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DRV8870 外部条件:原理图设计和手册要求一致,电流限制为1.3A,使用8KHz PWM 85%~100%占空比驱动IN1,IN2低电平。 驱动一个直流有刷电机,如果驱动线比较短(15cm),运行比较正常(速度30RPM),稍微加长几个cm,电机速度就变为几乎不动了,测量OUT1波形,发现只有大约20us为高电平,正常应该有100us高电平,不知道为啥会这样。




您好,
为了更好地解决您的问题,您能否提供以下信息: