This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8434S: nSCS FOR SPI COMMUNICATION

Part Number: DRV8434S
Other Parts Discussed in Thread: DRV8434, , DRV8434A

i use spi  communication between MCU and drv8434s, but the MCU do not have enough IO , so i would like the nscs pin to connect to ground to make the drv8434s is always selected( drv8434 is the only one device to communicate with MCU through SPI), but in drv8434s datasheet, i found the  below description , does this means i need to pull nscs pin high during the communication? if i keep it low, the spi communication will failed?

x 出现错误。请重试或与管理员联系。