This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: 低速状态希望达到平稳静音,调试遇到问题

Part Number: DRV8711

在使用drv8711的时候,希望达到低速平稳静音的效果,但是经过调试之后没有达到理想的效果,现将问题记录,希望得到建议和支持。

问题1:如下图Figure 1蓝色箭头所示,Itrip decrease在进入slow decay之后,图中电流任然上升了一段时间,按我的理解应该在进入到slow decay之后电流立刻开始下降,所以这里是有什么我理解错误的地方吗?

 

Figure 1datasheet中关于Itrip的图

问题2mixed-decay模式在电流零点附近的问题

测试条件如下:

  1. 步进电机参数如figure2所示,型号为 SST59D5305,图中黄色标注
  2. MOS管的型号为 NCEP065N10GU_N100V90A_DFN5X6
  3. drv8711寄存器配置如下

ctrl    reg: 0x341

torque reg: 0x178

off    reg: 0x20

blank  reg: 0x132

decay  reg: 0x301

stall   reg: 0x10f

drive  reg: 0xaa0

Figure 2 步进电机参数

Figure 3所示,示波器通道1(黄色)为高端,示波器通道2(青色)为低端,示波器通道3(紫色)为高端,示波器通道4(绿色)为低端;通道1和通道2H桥一边,通道3和通道4为一边。

 

Figure 3MOS管栅极驱动电压波形

 

Figure 4:电机静止时,电流0点附近,仅4通道替换为线圈电流,其他三通道保持不变

Figure 5:电机静止时,电流0点附近放大,仅4通道替换为线圈电流,其他三通道保持不变

Figure 6:电机静止时,电流0点附近,MOS管的动作

Figure 7:电机运行时电流波形

Figure 8:电流0点附近异常,黄色fault脚,绿色电机线圈电流

Figure 4568中可以看到,在电机静止的情况下,变化的幅值有了变化,我不清楚这样变化的原因是什么?

因为是在mixed-decay模式,从图中可以看到,像是在fastDecay之后并没有进入slowDecay,取而代之的是把4mos管全部关闭了Figure6,导致电流继续下降(mos管的体二极管),这是因为drv8711检测到了什么异常然后关闭了mos吗?但是fault脚的电平并没有变化,所以我不清楚这样的原因是什么,还请解答。而且在figure8所示的情况下,噪音很大。

问题3force fast decay at all times 电机电流低频变化

在这个模式下,在电流0点附近电流会好一些,但是电机的电流会低频的变化,而且PWM的频率很高(因为off寄存器的值很小),噪音也很明显。

Drv8711参数配置如下:

ctrl   reg: 0x341

torque reg: 0x178

off    reg: 0x3

blank  reg: 0x180

decay  reg: 0x201

stall  reg: 0x10f

drive  reg: 0xaa0

Figure 9force fast decay模式下电机运行时的电流波形

Figure 10force fast decay电机静止,4通道线圈电流变化

我也尝试了其他的decay模式,但效果也并不是很好,还请指导该如何调试,谢谢。

x 出现错误。请重试或与管理员联系。