This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8873-Q1: 50KHZ带载发烫

Part Number: DRV8873-Q1
Other Parts Discussed in Thread: DRV8873

各位老师好,现在我们用DRV8873带载非常烫,测试条件如下

1、供电12V,

2、单路带载电流1.5A

3、PWM驱动频率 50KHZ

温升很快会到100度左右,当我们降低频率到20KHZ的时候,温度会讲到90度左右,

问题:  1:DRV8873手册上面是支持到50KHZ的,为什么会烫,是不是我电路周围的器件搭配的不合理?

              2:我的负载要求是50KHZ,否则会有异响,除了降低频率有没有其他的办法解决发烫的问题?