Part Number: MCF8316A
hi, Ti vendor,
MCF8316A 的datasheet中MAX_SPEED 寄存器的定义如下:

请教下, MAX_SPEED 的值与电机的实际转速(假设单位r/min)要如何换算
是否MAX_SPEED 的值就是电机的目标转速, 例如设置MAX_SPEED = 100, 电机的转速是100r/min吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如您给的图中,应将 MAX_SPEED 配置为所需的最大电机转速,单位为 Hz。 要转换为 RPM,您需要获取电机的极数,然后使用以下公式:

例如,如果电机有12个磁极(6个磁极对),并且 MAX_SPEED 设置为100Hz,那么则表示最大速度(以 RPM 为单位)设置为100 * 60/6 = 1000RPM。 启用速度环路,意味着在100%输入速度命令下,器件将尝试将电机速度调节至1000RPM。 在输入速度命令为50%时,器件将尝试将电机转速调节到500RPM。