This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RS: 1

Part Number: BOOSTXL-DRV8323RS


各位技术人员好!我在使用DRV8323RS的时候,出现了很多问题。1.在与DRV8323RS通信的时候 读取错误状态寄存器的值 分别为0x0080 0x0040 分别是VM 欠压闭锁(UVLO),电荷泵欠压 (CPUV),我的供电电压是9V,通过万用表测得电荷泵电压是17V,其他寄存器读出来得初始值全部正确,这让我很困惑,明明一切都没有问题,nFault引脚也没有被拉低。2.当电压加到24V得时候,芯片明显发热,在不到2,3s的时间内发展到烫手的地步,外围没有接mos,并且伴有啸叫的声音。十分困惑,希望技术人员能给予支持!