This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8434A: DRV8434A 电机不转问题

Part Number: DRV8434A


1. 今天发现电机不转。检查发现电源为15.8V,正常,SLEEP,ENABLE 为高,FAULT,TRQ,STL_REP为 低,M0,M1为高,

2. 检查发现CPL,CPH管脚和正常的波形不一样,正常板子有脉冲波形,现在的板子没有

3.输出管脚AOUT1,AOUT2,BOUT1,BOUT2正常板子有2.4V输出,但现在的板子没有。,

现在我想知道。CPL,CPH波形不对,影响我输出吗?电机没有锁定,也是这个原因吗?

如果是,是我们焊接问题?还是这个IC被弄坏了?

谢谢