Part Number: DRV8301
Hello, TI teams
我们正在使用DRV8301-HC-EVM REVD硬件和InstaSPIN_MOTION_F2806xM软件识别我们BLDC参数并进行驱动(电压12V 8极12槽无刷电机)
在测功时我们设置Motor Max Current为30A,但在测功机上测试并当扭矩达到0.3Nm时,转速就掉落为0rpm,并且显示输出电流只有十几A,是不是有什么参数需要设置或者软件里面参数需要修改?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8301
Hello, TI teams
我们正在使用DRV8301-HC-EVM REVD硬件和InstaSPIN_MOTION_F2806xM软件识别我们BLDC参数并进行驱动(电压12V 8极12槽无刷电机)
在测功时我们设置Motor Max Current为30A,但在测功机上测试并当扭矩达到0.3Nm时,转速就掉落为0rpm,并且显示输出电流只有十几A,是不是有什么参数需要设置或者软件里面参数需要修改?
您好,
感谢您对TI产品的关注!为了更有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上(https://e2e.ti.com/p/addpost),将由资深的英文论坛工程师为您提供帮助。