This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

推杆电机的电流是否会有倍率关系,影响到DRV8874芯片电流阈值。

Part Number: DRV8874


我使用DRV8874芯片实现一个过电流保护的功能,PMODE=逻辑低电平,Rimode = 62KΩ至GND,Ripropi=1.8KΩ,按照公式上计算的电流阈值约为1.8A。当我接上推杆电机时,电机推出时nFAULT被拉低了,可实际上我的可调电源显示电流值为0.6A时,nFAULT就被拉低了。是否跟电机本身特性有关,还是说我的电流阈值计算错了?因为我使用全模组电阻时,则不会出现电流为0.6A时,nFAULT被拉低的情况。

  • 听起来可能存在与电机相关的初始浪涌电流。 电动机数据表中应该有一个说明电动机的浪涌或失速电流的规格。 当销杆到达行程末端时,可能会"失速"并消耗更多电流。 设备在6A左右达到OCP,这意味着电流需要超过6A,超过3us的破波时间。

    如果可能,您能否捕获输入,输出和电源电压以及电流(如果您有电流探头)?