This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8411: The problem of motor output pulse

Part Number: DRV8411


This signal was captured from the OUT1-4 pins of the DRV8411   However, once it was sent to the motor, it didnt rotate at all.

This is the waveform for each pulse,Is this signal all right?

There’s another issue: when the pulses are emitted, the chip’s power consumption is extremely low Not even 1mA of current

Could someone help answer these questions? Thank you very much!

plzzz