Part Number: DRV8411
This signal was captured from the OUT1-4 pins of the DRV8411 However, once it was sent to the motor, it didnt rotate at all.

This is the waveform for each pulse,Is this signal all right?

There’s another issue: when the pulses are emitted, the chip’s power consumption is extremely low Not even 1mA of current
Could someone help answer these questions? Thank you very much!
plzzz