Part Number: DRV8231
VM=28v,串联上1.5Ω的电阻,VREF=3.3v,ISEN引脚串联0.2Ω的电阻,静息电流26mA。外部中断发送指令,同时改变12个DRV8231的输出状态,此时VM=28v下的电流会为0再恢复26mA,重启芯片,这是为什么呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,根据您的描述,建议您从以下方面排查故障。
1. 观测INA1 INA2是否稳定,可以考虑增加驱动门。
2.VREF信号驱动能力是否足够,是否有抖动,可以考虑增加驱动buffer。
3.电源是否稳定,电路图中没有看到电源引脚处放置退耦电容。
4.Layout 布局不合理导致信号干扰,参见手册Figure 11-2. Layout Recommendation