This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8231: 同时改变12个DRV8231的输出状态时,会发生重启

Part Number: DRV8231


VM=28v,串联上1.5Ω的电阻,VREF=3.3v,ISEN引脚串联0.2Ω的电阻,静息电流26mA。外部中断发送指令,同时改变12个DRV8231的输出状态,此时VM=28v下的电流会为0再恢复26mA,重启芯片,这是为什么呢

  • 您好,根据您的描述,建议您从以下方面排查故障。

    1. 观测INA1 INA2是否稳定,可以考虑增加驱动门。

    2.VREF信号驱动能力是否足够,是否有抖动,可以考虑增加驱动buffer

    3.电源是否稳定,电路图中没有看到电源引脚处放置退耦电容。

    4.Layout 布局不合理导致信号干扰,参见手册Figure 11-2. Layout Recommendation

    https://www.ti.com/lit/ds/symlink/drv8231.pdf