Part Number: DRV8813
Hi All,
How much current can the DRV8813 chip withstand? Will it affect the chip life? Is there any test data to prove it?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Max Continuous motor drive output current is 2.5A.
Stresses beyond this Maximum Ratings may cause permanent damage to the device. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability and life.
The data is obtained through test, but the test data is not publicly available.