DRV8813: Withstand current

Part Number: DRV8813

Hi All,

How much current can the DRV8813 chip withstand? Will it affect the chip life? Is there any test data to prove it?

Best Regards

  • Hi,

    Max Continuous motor drive output current is 2.5A.

    Stresses beyond this Maximum Ratings may cause permanent damage to the device. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability and life.

    The data is obtained through test, but the test data is not publicly available.