This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8214EVM: GUI VM read wrong value

Part Number: DRV8214EVM


Hi team,

when I test DRV8214EVM, I connect 10V input to J8.

I utilized a multimeter to test the voltage between VSUP and VM and GND at 10V.

But, I read VM is 5.7V at GUI.

How do I use the GUI to read accurate data?