This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8434S: TRQ_DAC的问题

Part Number: DRV8434S


您好,

1.现在我发现一个新问题,再电机运转过程中,对CRTL1寄存器的TRQ_DAC[3:0]进行修改,无论我尝试升高或降低电机电流,此时电机将不再运动,并发出蜂鸣声,请问这是正常的吗?

是否不应该在电机运转TRQ_DAC?

2.当我试图增大CRTL1寄存器的TRQ_DAC[3:0],此时电机发出了噪音,其他值不变的情况下,TRQ_DAC越大,噪音就越大,当我把TRQ_DAC降低到37.5%以下,将不再有噪音

此致

     感谢

  • 您好,

    1.TRQ_DAC设置将数据表中所述的IFS电流从100%更改为6.25%。它可以动态更改。请记住,电机输出扭矩与IFS电流成正比。如果TRQ_DAC减小,电机扭矩也可能减小并可能使电机失速,特别是在变化明显不同的情况下。一旦电机失速,根据步进电机的行为特性,可能必须停止并重新启动。

    2.如果步进电机被过度驱动,电机将发出过大的声音,并且还会发出很高的噪音。必须设置VREF和TRQ_DAC,以实现电机的正确IFS值。使用的VM电压是多少?电机的IFS额定值(电机数据表将有所帮助)、使用的uStep模式、步进率、VREF输入、TRQ_DAC设置。你能分享一下这些条件下的电流波形吗?