This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329A: 总是小概率出现ABN_BEMF故障。

Part Number: MCF8329A


 尊敬的技术团队,大家好!提前祝大家中国新年节日快乐!

我遇到的问题是:在电机起步阶段,总有1%到2%的几率出现电机起步失败,出现ABN_BEMF故障。起步失败时:电机抖动后不旋转,然后出现高频振铃声音。

如果禁用LOCK2_EN,会1%到2%的几率起步失败时:电机抖动后不旋转,然后出现高频振铃声音。

我经过大量的调优,不管哪种启动方式(首循环,IPD),都无法解决这个问题。

我使用的电机信息不全,已知:1KW,48V,14极。启动时有一定的负载。不能空转。我的电机L,R,BEMF经过MPET例程获得。

我尝试更改的数据如下:

AUTO_HANDOFF_MIN_BEMF=100MV.

加大或者减少MOTOR_BEMF_CONST。

ABNORMAL_BEMF_THR=70%。

调试以下参数会直接LOCK_LIMIT故障,我的增益是20V/V.  电流阈值80%。

1.OPN_CL_HANDOFF_THR大于6H.

我需要帮助的问题主要就是小概率ABN_BEMF故障。

提前感谢帮助我的人,祝愿你天天开心!