This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电机从低速加速到高速,提速反而变慢了



补充:

我的工程是自己制作一辆两轮电动车。

经过大量调试,减少了首循环的速度,和开环的加速度,让开环到闭环的时间尽可能加长,可以解决以上问题,但是我又出现了新的问题。

电机30%占空比启动,电机开始正常运转550RPM,0-目标速度550RPM大约需要不到1秒钟,在此阶段,我尝试加大占空比到100%占空比,结果提速非常非常慢!

电机100%占空比启动,也就1秒多一点就可以到达目标速度1600RPM。我不知道为什么电机从低速加速到高速,提速反而变慢了。

我现在闭环加速度的寄存器配置为:{0x50,0x00,0x88,0xB8,0X81,0x29,0x0A,0x88};

           开环的配置为:{0x50,0x00,0x86,0x98,0X80,0x00,0x1D,0x09};

电流增益调至40V/V.

救救我~!