Part Number: DRV8311
我使用stm32G431单片机和DRV8311P芯片来驱动无刷有感电机,使用tSPI的通信控制方式。
1.能否给提供一个STM32单片机C语言的相关控制例程?
2.SPI的英文手册中寄存器控制命令较多,能否提供一个精简的中文版的可以使电机运转的寄存器命令文档?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 没有和STM32相关的,有和TI自己的MCU相关的以及芯片评估板对应的GUI。
见下方链接“设计和开发”部分
DRV8311 数据表、产品信息和支持 | 德州仪器 TI.com.cn
2.没有这类文档,
可以看评估板的手册,通过GUI操作。
1.我们使用DRV8311的时候,SOA引脚输出电流的波形只有下半边波形,和手册里的案例不一样,能给分析下是什么原因吗?
下图波形测量引脚为SOA和SOB;

2.我们分析电路图,电流采样电路在mos管的底边侧,如下图。得到的电流为什么会出现正负交替变化的波形,请帮助分析下。

3.我们在做BLDC控制时,寄存器配置 PWM_STATE Register (Offset = 1Ch) [Reset = 0777h] ,我们配置的六步换向使用的是1和6交替开关mos管实现六步换向,这样使用电机可以转起来,使用上有没有问题。