Other Parts Discussed in Thread: DRV8303
连接24V直流电源并将ENABLE引脚拉高后,nFault引脚为高电平,但nOCTW引脚一上电即为低电平。PVDD为24V,但GVDD无电压输出,DVDD为4V且有较大纹波,AVDD为7.11V。

以上是drv8301的原理图,nfault与noctw处连接的mosfet是n沟道的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有趣的是,GVDD没有输出,这可能是供应GVDD的电荷泵发生了故障。当PVDD为5-15V时,以及当PVDD高于15V(>15V)时,您能否重新测量/提供电荷泵引脚上放大的电压波形?我想比较一下它们在问题变得明显的不同范围内是如何运作的。
4V的DVDD意味着它违反了引脚的绝对最大值

我不确定DVDD的内部块也负责供电,但在4V时,内部块有可能损坏。你能在测试过程中使用新的IC吗?
这些FET背后的原因是什么?

此外,如果您没有使用降压,保持所有降压引脚浮动应该没问题,但我们确实有其他没有降压的设备可能更适合此应用程序?例如DRV8303或DRV832x系列(例如DRV8323S)等较新产品。

你好,检测发现CP1和CP2引脚间电容两端电压如上图所示,

gvdd引脚电压如上图所示,除此之外,还测量了CP1、CP2引脚的对地电压,均为40mV左右,也就是说,GVDD、CP1、CP2均基本未输出电压。
两个mosfet的作用是故障指示灯电路,当没有出现故障的时候,灯会亮起,现在的情况是一接电源nfault引脚即报错。
已经更换过一次芯片,但更换后出现同样的问题。(未使用drv8303是由于购买零件时,库存不够)
下图展示了完整的电路原理图,5V、3.3V的供电未有问题,PVDD引脚接24V电源时也显示24V电压值。

不,事实上,PVDD、GVDD、CP1、CP2、DVDD中,只有PVDD的电压是正常的(24V),其他引脚中,DVDD输出过大(4V),而CP1、CP2、GVDD几乎没有电压输出