Other Parts Discussed in Thread: LMV431
用手册推荐电路,做恒压源输出稳定。当我改为恒流源时输出出现断续模式,波形如下图。具体实现是芯片按照手册的恒流模式,但反馈我用的自己搭建的电路,在输出电容后级网络上串联电流采样电阻,经运算放大器调理后输出到FB引脚。修改Rramp、Ccomp、Rcomp也没有明显效果。

波形中蓝色为输出电容电压,黄色为FB引脚电压,观察过驱动波形也与此同步相应变化。芯片引脚Cres接芯片输出VCC(约7V)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
多谢您的分析,一会我再检查一下反馈回路,这么用没问题我就放心了。峰峰值8.08V是输出电容上的电压,FB信号是黄色波形,每格500mV,运放电源是±15V,我检查过没到运放饱和。
现正在测试手册推荐的利用LMV431实现恒流的方案,恒流也比较稳定,但碰到一个问题:DC输入是24V,输入电压最高被限制在13V,上不去了。检查上管驱动脉宽大概50%且很稳定,像是脉宽被限制了,类似于逐周波限制,但测试FB引脚电压(电压反馈)只有0.4V,Cramp三角波最高0.6V,也没有到1.2V限值,LMV431参考端电压0.5V左右,8550也没有打开,Rs为5mΩ,改为2.5mΩ也没变化。当前频率为100kHz。麻烦您帮忙给分析分析。