This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5190: 做Buck 转换器输出电压只有5V疑问

Part Number: LM5190


做Buck 转换器:

输入46-50V,设定电压输出为43.6V(外部100K/1.87K电阻器),设定恒流8A。图纸如下

出现的现象是:

1.无论是空载还是带载情况下输出只有5V左右;

2.监测VCC电压,启动瞬间有一个跳变之后立即变为0V

3.监测FB引脚电压,只有0V左右

4.监测MOS上下管驱动波形,下管基本正常,上管波形幅度很低

请帮忙分析原因?