在大电流路径使用这款芯片时VIN和VOUT之间总会存在约24mV的基础压降,这个压降不是由MOSFET的Rds(on)引起的。随电流上升,压降增长很缓慢,增长斜率几乎和MOSFET的Rds相等。通过实测数据拟合可以预见,在电流50A时,损耗功率达到2.4W,发热严重。请问这个压降是如何产生的,怎么避免?
如图,1-7A数据为实测,损耗为推测。原理图如下
MOSFET型号是HYG012N08NS1TA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在大电流路径使用这款芯片时VIN和VOUT之间总会存在约24mV的基础压降,这个压降不是由MOSFET的Rds(on)引起的。随电流上升,压降增长很缓慢,增长斜率几乎和MOSFET的Rds相等。通过实测数据拟合可以预见,在电流50A时,损耗功率达到2.4W,发热严重。请问这个压降是如何产生的,怎么避免?
如图,1-7A数据为实测,损耗为推测。原理图如下
MOSFET型号是HYG012N08NS1TA
负载和栅极电压是相关的。
使用2x0.9mohms MOSFET,在50A下,功耗应为1.1W。这可以通过(I^2Rds_on)方程计算得出。
在7A下,仅从(IV)方程来看,功耗似乎为193mW。