电源拓扑: 一级DCDC 输出5V → PMCI TPS6521905-Q1
睡眠模式下:关闭一级DCDC EN脚 关断5V
TPS6521905-Q1 VSEL配置为DDR3供电,硬件上10K上拉至MCU VCC(3.3V), 输出1.35V
在低功耗模式下,一级电源DCDC使能关闭,5V不输出,但DCDC_5V存在2.2V电压,排查:将VSEL上拉去掉,睡眠模式下DCDC_5V=0V
hlep!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电源拓扑: 一级DCDC 输出5V → PMCI TPS6521905-Q1
睡眠模式下:关闭一级DCDC EN脚 关断5V
TPS6521905-Q1 VSEL配置为DDR3供电,硬件上10K上拉至MCU VCC(3.3V), 输出1.35V
在低功耗模式下,一级电源DCDC使能关闭,5V不输出,但DCDC_5V存在2.2V电压,排查:将VSEL上拉去掉,睡眠模式下DCDC_5V=0V
hlep!
你现在的问题是你的一级DCDC5V输出网络在关断的情况下仍有输出,排查发现是VSEL的上拉电阻导致的?
请提供详细的系统框图和电路原理图。
当VSEL被拉到3.3V并且VSYS(5V)被移除时,我看到VSYS保持在1.1V的高电平,当VSYS被拉到GND时,VSYS变为0.75V。
不同引脚之间总是有内部本征结型二极管,对于没有电源但其他引脚被拉高的PMIC来说,这不是正常的应用。
当DCDC_5V变为2.2V时,PMIC是否以1.35V为DDR3供电?
PMIC VSYS UVLO下降约为2.2V,因此我预计PMIC应该关闭。
很高兴知道,当DCDC在睡眠模式下关闭时,PMIC输出为0V。
数据表中提到,正常运行时,I/O引脚电压不得超过VSYS。
为了避免这种情况,将VSEL拉到GND是可以的,但要让Buck3在1.35V下为DDR3供电,需要将Buck3_VSET设置为1.35V,同时将VSEL拉到GND。
关于Buck3电压与VSEL配置,请参阅数据表VSEL_SD/VSEL_DDR配置选项表。