This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560B: 芯片通过调整RT引脚电阻,没办法改变芯片的工作频率。

Part Number: TPS54560B


各位TI专家:

芯片在使用过程中,输出负载电流变化较快,导致电源纹波较大。

想通过调整RT引脚电阻,调整开关频率来尝试改善纹波,但是实际测试时发现,分别使用100K、150K、200K时,开关频率都是在384KHz。

电路设计输入电压24V,12V输出,电流3A;请问一下无法调整开关频率是什么原因?