This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq76920+bq78350+bq76200

Part Number: BQ78350
Other Parts Discussed in Thread: BQ76920, , EV2400, BQ76200

您好!最近使用bq78350做为bq76920的主机,但是出现了如下问题

1、bq76920的REGout可以正常输出3.3V,但是其与bq78350相连的ALER引脚无信号输出,是否会影响俩款芯片之间的通信?

2、bq76920与BQ78350连接的SCL,SDA引脚已通过上拉电阻上拉至REGout,且通过示波器观察SDA和SCL引脚有信号在传输,但是通过EV2400与BQ78350通信发现BQ78350的Voltage和CELL1-5的电压显示均为0,请问应该如何解决?可否提供相关资料?

3、BQ78350的BAT和VEN引脚参照BQ78350数据表设计电路,VEN引脚可以正常发出脉冲,BAT引脚显示有小于1V的电压,但是Voltage显示为0,是什么问题?示例电路Q8的集电极R47能否使用定值电阻?这个BAT引脚到底是什么作用?