Other Parts Discussed in Thread: UCC21520, INA240, TINA-TI, LM5146, CSD88599Q5DC
Background: I'm designing a 3kW DC-DC converter using 4 parallel MOSFETs (STF75N75), but 2 out of 4 keep overheating and failing. Current imbalance reaches 30% at full load—what am I missing?
1. Key Symptoms & Test Data
- Setup:
Full-bridge configuration, 150kHz switching
Gate drive: TI UCC21520 with 4.7Ω series resistors
Source resistors: 10mΩ/2W, connected to TI INA240 current monitor
- Abnormal findings:
️ Device #1 & #3 show 18A/12A current split at 60A total
️ Junction temp difference: 25°C between hottest/coldest MOSFET
️ Scope shows 50ns switching delay mismatch between devices
2. Potential Causes (Need Your Input!)
2.1 Component Matching Issues
- Question: Did I skip critical screening?
- Used random batch MOSFETs (Vth spread: 2.8V-3.5V)
- Rds(on) at 25°C: 75mΩ-82mΩ (data sheet says 75mΩ±10%)
- TI Expert tip: Should I use TI's parametric binning service for TMOS devices?
2.2 Layout Parasitics
- My PCB design:
️ 4-layer board, but source traces vary by 2mm length
️ Gate drive tracks routed on different layers (FR4 dielectric)
- Community challenge: How to model source inductance in PSpice? (Using TI's TINA-TI but no luck)
2.3 Thermal Runaway Mechanism
- Observed cycle:
- Device #1 carries more current → heats up
- Rds(on) increases 0.5%/°C → but current shifts to device #3
- Device #3 now overheats, repeats...
- Technical question: Does TI's LM5146 current-share controller handle dynamic thermal effects?
3. What I’ve Tried (Failed Solutions)
4. Desperate for Your Design Tricks!
- Specific help needed:
- Best practices for paralleling MOSFETs in TI reference designs?
- How to implement real-time current sharing with MCU (using TM4C129)?
- Recommended TI parts for high-reliability paralleling (drivers/sensors)?
5. Bonus: My SPICE Model & Layout Screenshot
(Attached: paralleling_test.zip with TINA-TI model + PCB gerber)
- Note: Thermal simulation shows hotspots at source via connections—could via inductance be the culprit?
Engineers, save my project! Tag someone who solved similar issues or drop your solution in comments.
#TICommunity #PowerDesign #MOSFETParalleling #CurrentSharing