This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133充电截止问题

Other Parts Discussed in Thread: BQ24133

我按照BQ24133评估板画的板,芯片也是按照评估板选型的!

咨询下,BQ24133在选用2CELL时,电池电压充到多大才会停止充电??

我选用的电池是2CELL,标准充电电压是8.4V

调试中发现一个问题,充电过程中,电池电压超过8.4V后,充电仍不会停止,一直充电到8.53V也不停止!

请教下这个问题怎么解决?

我在BQ24133中看到一个电池过压电压值,不清楚是不是电池充电截止电压。芯片资料第九页BAT OVER-VOLTAGE COMPARATOR 中 VOV_RISE( Overvoltage rising threshold)是VBAT_REG(8.4V)值的104%---8.736V,这个超过了8.4V,会不会对电池有影响?

 

  • 咨询下,BQ24133在选用2CELL时,电池电压充到多大才会停止充电??

    R. 如果启用了充电截止,锂电池是按照最小电流截止法,所以充电电流小于截止电流门限时截止。

        

  • 调试中发现一个问题,充电过程中,电池电压超过8.4V后,充电仍不会停止,一直充电到8.53V也不停止! 请教下这个问题怎么解决

    R. 是否按照datasheet page 9等这样的非可插拔结构来设计的?即TTC是否接地了,如果其接地,那么截止功能被禁止了。此时电池最终的端口电压取决于CV电压以及寄生参数/电池内阻的分压。

  • 我在BQ24133中看到一个电池过压电压值,不清楚是不是电池充电截止电压。芯片资料第九页BAT OVER-VOLTAGE COMPARATOR 中 VOV_RISE( Overvoltage rising threshold)是VBAT_REG(8.4V)值的104%---8.736V,这个超过了8.4V,会不会对电池有影响?

    R.VOV_RISE threshold 是指电池充电过程中如果电池端口电压上升到104%VBAT_REG后 触发的电池过压保护。

  • 请问你是几层板,可否贴上原理图看看,如果原理图没问题,看下在PVCC和PGND上直接用最短的线连一个10uF的陶瓷电容试下。

  • 你说的截止电流是这个? IQUAL(Termination qualification current) 这个值是2mA 我的情况是这样,电池充到8.4V的时候,电流约为0.4mA,充到8.56V时,是0.1mA,应为此时电压过高就停止充电了

  • 完全是按照BQ24133的评估板做的,无论原理图还是PCB

    TTC处接了103的NTC

    说到NTC了,温度过高后,应该停止充电的,但是我用热风枪吹NTC,使其温度升高,之后STAT处的指示灯闪烁,而适配器显示充电电流并未变化,仍为0.4mA多点

  • 4层板,基本按照评估板来做的 PVCC与PGND上的连线也和评估板上一致的

  • 补充,当电池电压高于8.4V后,出现过STAT口LED灯,关闭的情况,此时充电电流也为0

    但是这种情况只是偶尔,大多数情况是LED等闪烁,充电电流仍未100mA以上