Other Parts Discussed in Thread: BQ24195
你好,TI工程师:
我们的设备是用TI的BQ24195给锂电池充电,最近有客户退回返修发现BQ24195不能工作,测量电池电压大概3.1V左右,BQ24195的SYS引脚没有电压输出,导致系统没电不能启动。在外接电源的情况下SYS引脚也没有电压输出,电池也不能充电(测量外接电源的电流为0)。好像BQ24195进入某种状态(类似休眠或者死机),只有重新取下电池才可以恢复正常,然后把取下的电池再装上也可以正常工作,这时候也可以充电,BQ24195恢复正常工作。这种状况在我们这里不能重现,所以不知道在什么情况下才能出现。希望给出解决意见,谢谢!
上电寄存器配置:REG01--->0x00
Delay 100ms
REG01--->0x1B
REG05-->0x8A