Part Number: BQ27427
Other Parts Discussed in Thread: BQSTUDIO, BQ28Z620, BQ27Z746, BQ27Z558, BQ27Z561-R2
您好,我在用bqstudio进行参数配置的时候遇到了个问题:我之前一直用的是200mAh的锂电池,后面要换用18000mAh的标称3.7V锂电池组,容量超了上限,需要进行缩放,但由于pcb上的放电电流只有15mA左右,放电电流阈值想设置为12mA,当容量缩放至6000mAh,放电阈值缩放至4mA时,Dsg Current Threshold仍需要设为15000,会超过其2000的上限,如果要保持该值在2000以内,又会导致容量和电流的缩放比例不一致,请问这种情况应该怎么办呀
另外,还想请教一个问题,在id匹配和充放电周期学习完成后,pcb重新上电开机时,还需要再进行电量计的初始化和参数配置吗,如果此时再在stm32程序中配置或者修改参数,之前的周期学习会不会失效呀