This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02013: Regarding the disabling and enabling of TTPLPFC and CLLLC.

Part Number: TIDM-02013


Dear Expert,

I hope this message finds you well.

Since I can't post a new question on the forum, I'm bringing it up here.

While reading another article, I came across settings for starting and disabling TTPLPFC and CLLLC.

The article states the following:

- For CLLLC: It is disabled when `CLLLC_clearTrip = 0` and operational when `CLLLC_clearTrip = 1`.

- For TTPLPFC: It is operational when `TTPLPFC_AUTO_START = 0` and disabled when `TTPLPFC_AUTO_START = 1`.

However, I have not found any code that explicitly links the definitions of these two variables to the enabling or disabling of TTPLPFC and CLLLC. Could you please clarify whether the method described in the article is correct? If not, could you kindly provide the proper configuration methods for enabling or disabling TTPLPFC and CLLLC? Thank you for your assistance.

Sincerely,

Wang