Part Number: UCC27211
TI专家您好,
我这边想要一个高速的负载开关,开关频率在30khz,负载是一个LED,输入源是一个电流恒流源,能够提供10A,5-12V的恒流。
我是否可以用UCC27211DR来搭出这个电路,如果不行有其他推荐控制器及电路么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC27211
TI专家您好,
我这边想要一个高速的负载开关,开关频率在30khz,负载是一个LED,输入源是一个电流恒流源,能够提供10A,5-12V的恒流。
我是否可以用UCC27211DR来搭出这个电路,如果不行有其他推荐控制器及电路么?
感谢您对TI产品的关注!
关于你的咨询,UCC27211DR是一款高速推挽驱动器,理论上是可以满足你的需求的。
UCC27211可以高速驱动大功率MOSFET,但你还需要选择合适的栅极驱动MOSFET用于控制负载(LED)
主要挑战是整体电路的功率承载能力、散热和电路布局。
开关频率:30 kHz(日常大部分钳位驱动都能实现)
负载:LED(范围10A,5-12V)
高速切换,确保效率和控制准确,大电流驱动与散热.
10A负载需要选用低导通阻抗(Rds(on))的MOSFET件,确保在开关状态下产生的功耗最小。