This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211: 想要一个5A的10V的快速负载开关,开关频率在30Khz

Part Number: UCC27211


TI专家您好,

   我这边想要一个高速的负载开关,开关频率在30khz,负载是一个LED,输入源是一个电流恒流源,能够提供10A,5-12V的恒流。

我是否可以用UCC27211DR来搭出这个电路,如果不行有其他推荐控制器及电路么?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 感谢您对TI产品的关注!
    关于你的咨询,UCC27211DR是一款高速推挽驱动器,理论上是可以满足你的需求的。
    UCC27211可以高速驱动大功率MOSFET,但你还需要选择合适的栅极驱动MOSFET用于控制负载(LED)
    主要挑战是整体电路的功率承载能力、散热和电路布局。

    开关频率:30 kHz(日常大部分钳位驱动都能实现)
    负载:LED(范围10A,5-12V)
    高速切换,确保效率和控制准确,大电流驱动与散热.
    10A负载需要选用低导通阻抗(Rds(on))的MOSFET件,确保在开关状态下产生的功耗最小。