This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Max Error 更新条件

Part Number: BQ4050

hi

请教一个问题达到bq4050 Max Error 更新条件是什么?是不是放电到截止电压才更新,还是说放电到EDV2 7%电量和FCC一起更新呢?

另外一个问题:

一,如果设定Fixed EDV 固定 EDV   也需要Max Error更新到2%或者8%吗?我测试好像这个Max Error不会更新,一直保持100%,是什么原因呢?