This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: 帮我看一下cedv参数 常温测试过程中, 为什么算出来的 edv2 电压 很大,过早校准 7%,有什么问题

Part Number: BQ4050


     GPC CEDV tool, rev=61
Configuration used in present fit
ProcessingType=1
NumCellSeries=1
CellTermV=2500
ChemType=6
LearnSOC%=7
FitMaxSOC%=10
FitMinSOC%=4
ElapsedTimeColumn=0
TemperatureColumn=3
CurrentColumn=2
VoltageColumn=1


CEDV parameters resulting from the fit. If EDVV bit is set to 1, EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash

EMF 3157
EDVC0 253
EDVC1 0
EDVR1 1045
EDVR0 885
EDVT0 4991
EDVTC 11
VOC75 3866
VOC50 3663
VOC25 3554


Recommended SOC deviation tolerance at EDV2 point is < 5% for low temperature and <3% for room and high temperature

Deviations for this set of parameters are given below for each file

file SOC error, % pass
roomtemp_lowrate.csv -2.08941136367851 1
roomtemp_highrate.csv -0.925142641434015 1
hightemp_lowrate.csv -0.0537557638652277 1
hightemp_highrate.csv 1.36350489849546 1
lowtemp_lowrate.csv 3.3600633542309 0
lowtemp_highrate.csv -6.10985602082541 0

Warning: Deviation is above recommended level. Retry the fit with different settings, or proceed on your own risk if the accuracy is acceptable for your application